Attributes (HD Constant Flow Setpoint) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the HD Constant Flow Setpoint modules.

Table 1. HD Constant Flow Setpoint Attributes

Name

Type 1

Description

Default Value

CD Percent

 

Contains a percentage that spans between the max and min flows. 0% maps to max flow and 100% maps to min flow.

0.0%

Deck Max Flow

 

Contains the maximum deck flow setpoint.

500 l/s, 1000 cfm

Deck Min Flow

 

Specifies the minimum deck flow setpoint.

0 l/s, 0 cfm

Flow Percent

V

Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow and 100% maps to max flow.

Display Units: %

Flow Setpoint

V

Contains the desired Flow Setpoint. This is the setpoint for another activity, typically the Supply Damper Control module.

0 l/s, 0 cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)