Module Use in Applications (Flow Setpoint [VAV Single Duct]) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees in the software use the individual modules in this group using the name in the following table.

Table 1. Flow Setpoint (VAV Single Duct) Uses in Application System Selection Trees

Module Instance Name

Applications

Supply Flow Setpoint Control v51

VAV Single Duct Applications

Note: The Flow Setpoint (VAV Single Duct) module instance appears in the Output Control category; however, to add a new Flow Setpoint (VAV Single Duct) module from the palette (Module Selection dialog box), select New from the State Generation header right-click menu.

To see a module's connections and how modules interact with it, view the Connections table.