Enable Modules - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

All Network Inputs with a -EN name are always paired with an Availability type State Generation module. These inputs drive a state condition in their paired State Generation module that is captured in the State Selection Table.

The primary use of the Enable modules is to allow system-wide logic to determine if the Central Heating and Cooling Central Plants are providing Hot or Chilled Water to the devices. For example, if the HTG-EN Network Input is set to a False state, the Box Heating is Available Pass Through State Generation module does not allow the Heating Valve to open on a VAV Box.

The following table describes the Enable Network Input modules and lists the applications in which they are used.

Table 1. Enable Network Input Modules

Name

Description

Applications

BASIN-C

Drain Basin - Provides input to the Humidification Scrubber Output v51, Output Controller module.

CLG-EN

Cooling is Available - Provides input to one of the following modules:
  • Cooling Availability Determination

ECON-EN

Economizer is Available - Provides an input to the Economizer Availability Determination module.

HC-EN

2 Pipe is Available - Provides an input to the 2 Pipe is Available Pass Through State Generation module.

HR-EN

Heat Recovery is Allowed - Allows or locks out Heat Recovery operation where the actual suitability is determined locally to set the device for the heating or cooling operation.

HTG-EN

Heating is Available and Box Heating is Available - Provides input to one of the following modules:

Heating Availability Determination.

HUM-EN

Humidification is Available - Provides an input to the Humidification is Available Pass Through State Generation module.

All Air Handling Unit Applications

PH-EN

Preheat is Available - Provides an input to the Preheat Availability Determination State Generation module.

RH-EN

Reheat is Available - Provides an input to the Reheat Availability Determination State Generation module.

AllAir Handling Unit Applications

SUPHTG-EN

Supp Heating is Available - Provides an input to the Supplemental Heating is Available Pass Through State Generation module.

SYS-RESET

System Reset - Provides manual restart functionality.

ZNHTG-EN

Zone Heating Is Available - Provides input to the Zone Heating Availability Determination State Generation module

AHU Multizone (Mixed Air Dual Duct) Applications