Network Input Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Network Inputs module category appears in the Control View and lists the network inputs defined for the system. Network inputs are typically used to read and write values to and from a supervisory device or using peer-to-peer references between Field Controllers. When a network input is not integrated into the network, it uses its default value and can be commanded from the Commissioning mode. Network inputs connect into other modules or the State Table.

Network Input modules fall into one of the following categories:

See also N2 Compatibility Network Inputs in the N2 Compatibility Options section.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.