The following tables list the controllers and points that you can manually map into an N2 supervisor.
Note: The maximum limits of a General Purpose, Advanced Application, and VAV Controller are different from the maximum limits of N2 devices. Consider these limitations in addition to the guidelines in the following tables.
| Network Point Type | Network Point Address | Command Allowed | Can Map to NAE Objects |
|---|---|---|---|
| AI | 1–8 | Yes | AI, AO, MSI, MSO |
| AO | 1–8 | Yes | AI, MSO |
| BI | 1–8 | Yes | BI, BO
BI 7–8 can be mapped to Accumulator |
| BO | 1–10 | Yes | BO |
| ADF | 1–64 | No | AI, MSI |
| 65–256 | Yes | AI, AO, MSI, MSO | |
| ADI | 1–64 | No | AI, MSI |
| 65–256 | Yes | AI, AO, MSI, MSO | |
| BD | 1–64 | No | AI, BI, MSI |
| 65–256 1 | Yes | AI, AO, BI, BO, MSI, MSO |
| Network Point Type | Network Point Address | Command Allowed | Can Map to NAE Objects |
|---|---|---|---|
| AI | 1–40 | Yes | AI, AO, MSI, MSO |
| AO | 1–8 | Yes | AO |
| BI | 1–37 | Yes | BI, BO
BI 4 can be mapped to computer |
| BO | 1–14 | Yes | BO |
| ADF | 1–64 | No | AI, MSI |
| 65–256 | Yes | AI, AO, MSI, MSO | |
| ADI | 1–64 | No | AI, MSI |
| 65–256 | Yes | AI, AO, MSI, MSO | |
| BD | 1–64 | No | AI, BI, MSI |
| 65–256 2 | Yes | AI, AO, BI, BO, MSI, MSO |
| Network Point Type | Network Point Address | Command Allowed | Can Map to NAE Objects |
|---|---|---|---|
| AI | 1–6 | Yes | AI, AO, MSI, MSO |
| AO | 1–8 | Yes | AI, MSO |
| BI | 1–5 | Yes | BI, BO
BI 4 can be mapped to computer |
| BO | 1–8 | Yes | BO |
| ADF | 1–64 | No | AI, MSI |
| 65–256 | Yes | AI, AO, MSI, MSO | |
| ADI | 1–64 | No | AI, MSI |
| 65–256 | Yes | AI, AO, MSI, MSO | |
| BD | 1–64 | No | AI, BI, MSI |
| 65–256 3 | Yes | AI, AO, BI, BO, MSI, MSO |
1 BD point addresses 245–248 are reserved for user-defined data storage points.
2 BD point addresses 245–248 are reserved for user-defined data storage points.
3 BD point addresses 245–248 are reserved for user-defined data storage points.