Math - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Math folder in the control block palette contains blocks that perform mathematical functions on one or more inputs, producing a single output. The number of inputs to a Math block depends on the number of inputs supported by the type of math function. The Logic View allows you to add multiple connections to the output of the block.

The Math primitive provides the following reliability values: Math Overflow, Math Underflow, Divide by zero, Not a number, Math Error.

Table 1. Math Blocks

Type

Description

Inputs (Float) 1

Outputs (Float)1

Absolute Value

Absolute Value

I1

Present Value

ACOS 2

Arc Cosine

I1

Present Value

Add

Add

I1

I2

Present Value

ASIN2

Arc Sine

I1

Present Value

ATAN2

Arc Tangent

I1

Present Value

COS2

Cosine

I1

Present Value

Divide

Divide (I1/I2)

I1

I2

Present Value

Exp

Exponent (el1)

I1

Present Value

LOG

Natural Log (LN, LOGe, or LOG base e)

I1

Present Value

LOG10

LOG10

I1

Present Value

Multiply

Multiply

I1

I2

Present Value

Negate

Negative

I1

Present Value

Power

Power (I1I2)

I1

I2

Present Value

Round

Rounds to nearest 1s

I1

Present Value

SIN2

Sine

I1

Present Value

SQRT

Square Root

I1

Present Value

Subtract

Subtract

I1

I2

Present Value

TAN2

Tangent

I1

Present Value

1 The inputs and outputs of this block are exposed for connection by default.
2 This block uses radians instead of degrees. To convert from degrees to radians, multiply the value by 0.0174533, that is, pi/180.