Module Use in Application (MAX) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees in the software use the individual modules in the following table.

Table 1. MAX Blocks Used as Modules

Module Instance Name

Applications

Max CHW Flow Max

Central Cooling with Optimization Applications

Required CHW Flow Max

Central Cooling with Optimization Applications

Required CW Flow Max

Central Cooling with Optimization Applications

Required Tower Flow Max

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.