The Activity Inputs folder in the control block palette contains Boolean, float, and enumeration input blocks. Use Activity Inputs to provide an incoming connection point to custom logic modules.
Note: The tool automatically creates and configures the hierarchy table in a translation block when you connect an Activity Input block to an Activity Output block of a different type (Boolean to two-state Enum or two-state Enum to Boolean).
|
Type |
Description |
|---|---|
|
Input (Boolean) |
Provides a Boolean input for connection to other blocks in the logic diagram (True or False). |
|
Input (Enum) |
Provides an enumeration (Enum) input for connection to other blocks in the logic diagram. |
|
Input (Float) |
Provides a floating (Float) input for connection to other blocks in the logic diagram (numeric value). |