Coils (HP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Coils selection assumes that at least one compressor is created for a Heat Pump System.

During the Control Selection process, you must select the configuration of the reversing valves to determine if a reversing valve is enabled for heating or cooling.

The selection options for Coils are:

  • Condensate Alarm: This option adds a binary input for a condensate sensor that shuts down the cooling system when activated.
    • Shutdown on Alarm: This option places the system in shutdown mode when the Condensate Alarm is active.
  • Isolation Valve:This option controls an isolation valve for each heat pump.

    • Isolation Valve Status: This option monitors the status of the heat pump isolation valve.

  • Two Compressors-Reversing Valves: This option creates the required Output Controllers and Outputs for a two compressor system.

  • Supplemental Heating

    • One Stage

    • Two Stages