Economizer Suitability (HP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

When selected, the Economizer Suitability options create Proportional Damper Output Controller, Mixed Air Damper Output, and Minimum Position Determination Logic. The Economizer Availability Determination Setpoint module is also created and interfaced to the Economizer Suitability option selected.

The selection options for Economizer Suitability are:

  • Network Command

  • Binary Input (Enthalpy Switch)

  • Outdoor Air

    • Dry Bulb Temp Economizer

    • Temp & Enthalpy Economizer