Cooling (FC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following sections define the type of cooling coil in the fan coil.

Cooling cannot be selected if Common Heating-Cooling is selected.