Condensate Alarm (FC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This option provides a Binary Input to indicate the condensate drain is clogged. The cooling is disabled when the Condensate Alarm is active. The Shutdown on Alarm option shuts down the fan coil when the condensate alarm is active.