Fan Status Interlock with Zone Cooling (FC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This option is available only if a Stage Cooling Coil is selected. When selected, logic is created to monitor fan status through a binary input. The Airflow Status Determination (Flow Status Determination) module uses this status feedback to enable or disable the Staged Cooling Control (Cooling Staged Outputs v51) Output Controller.