Cycle During Occupied (FC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This option configures the Fan Determination State Generator module’s input for Fan Cycle to a Yes value, allowing the fan to turn off during Occupied if heating and cooling are both inactive. Otherwise, the Fan runs continuously during Occupied Mode. This selection is not available if the Fan Controlled By Other selection has been made.