Packages Tab - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. Hardware Definition - Packages Tab

Field

Description

Packages Information Table

Name

Name of the device associated with the package file.

Description

Region the package file was released for or the category of the package file.

Build Number

Build of the hardware package file.

License Status

License status of the package file. If the file is Unlicensed, the CAF can be opened as pseudo-artificial.

Import

Use to import new packages into your machine's package environment.

Close

Closes the dialog box.

Opens the Help system.