Set Maximum Quantity Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See the Defining Hardware section.

Table 1. Set Maximum Quantity Dialog Box
Field Description
Slider Bar (1 to 5) Use to set the maximum quantity of devices that appear in the quantity slider bar of the Add Devices dialog box.
OK Applies the changes and closes the dialog box.
Cancel Closes the dialog box without applying the changes.
Opens the Help system.