See the Modifying Points on an SA Bus Device section.
|
Field |
Description |
|---|---|
|
Add |
Use to select whether or not to add the point to the device. |
|
Type |
Point type. |
|
Function |
Point function. |
|
Data Type |
Point data type. |
|
OK |
Applies the changes and closes the dialog box. |
|
Cancel |
Closes the dialog box without applying the changes. |
|
|
Opens the Help system. |