Importing Package Files - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

Use the Import feature to import packages.

Procedure

  1. Click Define Hardware.
  2. On the Packages tab, click Import, and then navigate to the package file that you want.
    Note: Field controller packages show the status Licensed or Unlicensed in the Packages tab. If a field controller package is unlicensed, the CAF can be opened as pseudo-artificial.
  3. Click OK.