Natural Gas Items (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Natural Gas Items are:

  • Monitor Pressure Sensor (AI): This option measures pressure in the natural gas system.

  • Monitor Pressure Switch (BI): This option indicates if the natural gas pressure falls below the switch setting.

  • Monitor Flow Sensor (AI): This option measures flow in the natural gas system.