Modules (Custom/Monitoring Misc Status Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Misc Status Items selections load the following modules in this Control View column:

Inputs

  • DOORX-S (Door X Status BI, where X is 1-6): This Input is loaded when the Monitor Door Switch (BI) node is selected. Specific Inputs are loaded per switch.

  • MOTOR-S (Motor Status BI): This Input is loaded when the Motor Status (BI) node is selected.

  • SMKX-S (Smoke Detector X Status BI, where X is 1-6): This Input is loaded when the Monitor Smoke Detector (BI) node is selected. Specific Inputs are loaded per smoke detector.

See the Input Modules section.