Modules (Custom/Monitoring Medical Gas Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Medical Gas Items selections load the following modules in this Control View column:

Inputs

  • MGXPHI-A (Med Gas X High Pressure BI, where X is 1-6): This Input is loaded when the Monitor High Pressure Switch (BI) node is selected. Specific Inputs are loaded per switch.

  • MGXPLO-A (Med Gas X Low Pressure BI, where X is 1-6): This Input is loaded when the Monitor Low Pressure Switch (BI) node is selected. Specific Inputs are loaded per switch.

  • MVAC-A (Med Vacuum Alarm BI): This Input is loaded when the Monitor Medical Vacuum Alarm (BI) node is selected.

  • MVAC-P (Med Vacuum Pressure AI): This Input is loaded when the Monitor Medical Vacuum Pressure (AI) node is selected.

See the Input Modules section.