Medical Gas Items (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Medical Gas Items are:

  • Monitor Low Pressure Switch (BI): This option indicates if the pressure in a medical gas line drops below the switch setting.

    • 1 Switch (1 BI)

    • 2 Switches (2 BIs)

    • 3 Switches (3 BIs)

    • 4 Switches (4 BIs)

    • 5 Switches (5 BIs)

    • 6 Switches (6 BIs)

  • Monitor High Pressure Switch (BI): This option indicates if the pressure in a medical gas line exceeds the switch setting.

    • 1 Switch (1 BI)

    • 2 Switches (2 BIs)

    • 3 Switches (3 BIs)

    • 4 Switches (4 BIs)

    • 5 Switches (5 BIs)

    • 6 Switches (6 BIs)

  • Monitor Medical Vacuum Alarm (BI): This option indicates whether the medical vacuum system is in an alarm condition.

  • Monitor Medical Vacuum Pressure (AI): This option measures the pressure in the medical vacuum system.