Electrical Power Items (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Electrical Power Items are:

  • Monitor Status (BI): This option indicates power status.

  • Monitor Fault (BI): This option indicates when a fault condition is reported by the electrical panel.

  • Monitor Current (3 AI): This option measures the current for all three phases of electrical power.

  • Monitor Voltage (3 AI): This option measures the voltage for each phase to neutral.

  • Monitor Power Factor (3 AI): This option measures the power factor (ratio of real power to apparent power) for all three phases of electrical power.

  • Monitor KW (AI): This option measures KW power.

  • Monitor KWh (AI): This option measures KWh power.

  • Monitor Phase Failure (BI): This option indicates if any of the three phases of electrical power fail.