Modules (Custom/Monitoring Duct Items) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Duct Items selections load the following modules in this Control View column:

Inputs

  • DUCT-P (Duct Pressure AI): This Input is loaded when the Duct Pressure Sensor (AI) node is selected.

  • DUCTX-T (Duct X Temperature AI, where X is 1-6): This Input is loaded when the Duct Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • FILTX-S (Filter X DP Alarm BI, where X is 1-6): This Input is loaded when the Filter Status Diff Pressure Switch (BI) node is selected. Specific Inputs are loaded per switch.

  • HP-A (Duct High Static Fault BI): This Input is loaded when the High Duct Pressure Switch (BI) node is selected.

  • HT-A (High Temperature Limit Fault BI): This Input is loaded when the High Duct Temperature Alarm (BI) node is selected.

  • LP-A (Duct Low Static Fault BI): This Input is loaded when the Low Duct Pressure Switch (BI) node is selected.

  • LT-A (Low Temperature Limit Fault BI): This Input is loaded when the Low Duct Temperature Alarm (BI) node is selected.

See the Input Modules section.