Command General Equipment or Lighting (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Command General Equipment or Lighting are:

  • Command General Equipment or Lighting (BO): This option indicates the command to the equipment or lighting.

    • Status (BI): This option indicates whether the equipment/lighting is running/on based on the command for up to six systems.

    • Quantity

      • One

      • Two

      • Three

      • Four

      • Five

      • Six