Specifying Local Controller Display timeout settings - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget.
  3. Click Edit.
  4. Locate the Display Setup panel.
  5. In the Timeout Settings area, click the drop-down box to select an Idle Timeout value.
  6. In the Timeout Settings area, click the drop-down box to select a Backlight Timeout value.
  7. Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.