Selecting points to appear on Display pages or Idle page - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget.
  3. Click Edit.
  4. Select any point from the System Tree and drag it to the desired location on the Display Pages tree.
    Note: Select multiple points by holding down Ctrl while selecting items.
  5. Drop the selected points in the Display Pages Tree.
    Note: You can drop points on a folder or on a folder member. The new items appear at the end of the existing folder items or after the target folder member.
  6. Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.