Renaming folders in the Display - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget in the Features panel. The Display widget appears.
  3. Click Edit.
  4. Right-click any folder in the Display Pages tree, and then select Rename. Alternatively, you may select a folder, and then press F2.
    The Page Name dialog box appears.
  5. Type a name in the Page Name dialog box.
  6. Click OK. The new folder name shows in the Display Pages Tree.
    Note: For DIS1710 and DLK0350, the first three Display Pages folder names are standard and cannot be changed for the display. If you rename the Idle, Inputs/Outputs, or Parameters pages, the name change does not display.
  7. Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.