Procedure
- Start the tool and open the controller application.
- Select the Display widget.
- Click Edit.
- Locate the Display Pages panel.
-
Select the Export button (
) in the Import/Export area.
- Create a name and select a location for your file.
- Select Save. Your configuration is saved for future use.
-
Select the Import button (
) in the Import/Export area.
- Browse to your file location and select a file.
- Select Open. The Display Pages tree updates based on the configuration in the file.
Note: You will see an error message if the selected file is invalid or contains points that are not present in the current application.