Procedure
- Start the tool and open the controller application.
- Select the Display widget.
- Click Edit.
- Locate the Display Pages panel.
-
In the Customize area, click Create Page (
). The Create Page dialog box appears.
-
Enter a customized page name. The new page appears as the last folder in the Display Pages tree.
Note: The DIS1710 and DLK0350 setup allows up to 13 customized pages. Additional customized pages are not recognized by the device and do not appear accurately in the controller display.
- Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.