Viewing and Modifying System Selections - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Important: If you have already selected a system or opened a CAF in the tool, you can view and change the selections made. All previous user modifications are lost if you make changes to the system selections (lost changes include: sideloops, user added inputs, outputs, network inputs, network outputs, modules, changes in state tables, parameters, logic, and input/output setup). For information on the types of systems and selections available, see the User Interface and Applications sections.

See Rerunning System Selection in the Upgrading System Files section for guidelines on viewing and modifying system selection.