Viewing and Modifying Parameters - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Click the Parameters widget if not already active. See the Parameters description in the Perspectives section.
  2. Click Edit.
  3. Make changes to the parameters/attributes using the fieldes and drop-down menus and click Apply.
    Notes:
    • You cannot modify outputs of modules from the Parameters table.
    • You cannot save or switch modes while editing in the Parameters tab. Click Apply or Cancel before proceeding.