Making a Connection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. On the Connections tab, right-click an input or output that has no connections and select Make Connection. The Select Reference dialog box appears.
    Notes:
    • The left pane of the Select Reference dialog box is populated with only those modules that are available for connection.
    • A module output can have more than one connection (fan-out). A module input cannot have more than one connection (fan-in is not allowed).
  2. In the Filter box, type part or all of the node name to filter the results.
  3. Select an available module. The available ports appear in the right pane.
  4. On the right pane, select the input/output port in which to connect and click OK.
    Note: If you are having trouble making connections for loops, see the related entry in the Troubleshooting section.