Changing a Connection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
Controller Tool Help
- Product
- Controls > Control Tools > Controller Configuration Tool
- Document number
- LIT-12011147
- Version
- 15.0
- Revision date
- 2022-11-18
Procedure
-
On the Connections tab, right-click an input or output that has an existing connection and select Change Connection. The Select Reference dialog box appears.
Notes:
- The left pane of the Select Reference dialog box is populated with only those modules that are available for connection.
- A module output can have more than one connection (fan-out). A module input cannot have more than one connection (fan-in is not allowed).
-
In the Filter box, type part or all of the node name to filter the results.
-
Select an available module. The available ports appear in the right pane.
-
On the right pane, select the input/output port in which to connect and click OK.