Renaming a System - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

The steps to rename your system vary depending on your perspective. The following steps apply to editing the system name using the Classic View perspective. If you are using a different perspective, navigate to the details view of the Control Sequence object and begin at Step 2.

Procedure

  1. With a system open, click the System Information link on the status bar.
  2. Click Edit.
  3. In the Name field, type the desired name. Invalid characters include:

    : * ? " < > | / [ ] # @

  4. Click OK.
    Note: This option does not change the name of the CAF.