See the Logic Tab Screen description in the User Interface section.
In addition to the Zooming Icons in Table 1, you can also use the plus (+) and minus (-) keys to zoom in and out, and the arrow keys move up, down, left, or right. You can also use the scroll wheel to move up and down, hold the Shift key and scroll to move left and right, and hold the Ctrl key and scroll zoom in and out.
| Function | Description | ||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Zoom In |
Click the Zoom In icon from the Logic View diagram to zoom in on diagram details. | ||||||||
|
Zoom Out |
Click the Zoom Out icon from the Logic View diagram to zoom out of the diagram. | ||||||||
|
Fit To Window |
Opens the Fit To Window Menu from the Logic View diagram. The following table shows the Fit To Window Menu Icons
|