Setting the Default Element of a Module - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

Procedure

  1. Click the Set Default Element button in the Logic View toolbar or right-click within the white space of the Logic diagram and select Set Default Element. (Alternatively, right-click any block or node within the Table Data widget or BACnet Exposed widget and select Select Default Element.) The Default Element Selection dialog box appears.
  2. Select the radio button of the desired element and click OK. The default element appears black in the logic diagram.