Configuring the Line Segment Block - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

For information on the Line Segment block, see Calculation in the Logic section.

To configure the Line Segment block:

Procedure

  1. Double-click a Line Segment block. The Line Segment Details dialog box appears.
  2. Click Edit.
  3. In the Name field, type a new name to identify the block. This name appears in the logic diagram and replaces the Line Segment heading in the Details dialog box.
  4. In the Input Points and Output Points columns, select a cell and type the desired values.
    Note: The input points must be in increasing order.
    Tips:
    • To add a row, right-click a cell and select Insert Row.
    • To add 5 rows, right-click a cell and select Insert 5 Rows.
    • To remove a row, right-click a cell and select Delete Row.
  5. Click Apply.