Changing the Hidden Edge Label of a Connection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

See the Logic Tab Screen description in the User Interface section.

To change the hidden edge label of a connection:

Procedure

  1. Double-click the connection’s hidden edge label (numbered circle next to an Activity Input, Activity Output, block input, or block output: , , or ). The Hidden Edge Label dialog box appears.
  2. Type a name or number for the label and click OK. The label text changes as defined.