Use this dialog box to make changes to the labels in the block's name. See Renaming a Module and Renaming a Block.
|
Field |
Description |
|---|---|
|
User Name |
Specify a name for the module/block.
Note: If this field is blank, the Standard Name is used.
|
|
Standard Name |
Displays a Johnson Controls standard name for the module/block. |
|
OK |
Applies the name change and closes the dialog box. The name change appears in the Control View or Logic View. |
|
Cancel |
Closes the dialog box without applying the change. |
|
|
Opens the Help system. |