New System - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See Selecting a System (Creating a New System).

Table 1. New System Dialog Box

Field

Description

Intended Field Device

Shows all field devices that are compatible with the release mode displayed in the Release Mode drop-down list.

Note: If a field device is incompatible with a release mode it will be grayed out. A status displays if there are no available release modes for the selected field device.

Release Mode

Shows all release modes that are compatible with the field device selected in the Intended Field Device field.

Note: Upon selection of a device, the Release Mode drop-down list defaults to the earliest switchable release mode that is applicable to that device. A release mode does not appear in the list if it is incompatible with a field device.

Online Library

Use this option to download customized CAF files along with a sequence of operation, flow diagram, and points list.
Note: This feature is available to Technician licensed users only.

System Name

Use this option to enter a name for your new system.

System Type

Use this option to select the type of system to create. Options include (see Applications ):
  • Air Handling Units
  • Fan Coil
  • Unit Ventilators
  • Heat Pumps
  • VAV
  • Central Heating
  • Central Cooling Plants
  • Simple Central Plant
  • Custom Applications
  • Monitoring Supervisory Control Only

System Configuration

Use this option to select a configuration type for your new system. Options include (see Applications ):

Air Handling Units

  • Mixed Air Single Duct
  • 100% Outdoor Air Single Duct
  • Mixed Air Dual Duct
  • 100% Outdoor Air Dual Duct
  • Rooftop Unit
  • Multizone (Mixed Air Dual Duct)

Fan Coil

  • Blank: This system type covers all configuration options.

Unit Ventilators

  • Blank: This system type covers all configuration options.

Heat Pumps

  • Blank: This system type covers all configuration options.

VAV

  • Single Duct
  • Dual Duct
  • Subordinate Single Duct
  • Subordinate Dual Duct

Central Heating

  • Blank: This system type covers all configuration options.

Central Cooling Plants

  • Central Cooling
  • Central Cooling with Optimization

Simple Central Plant

  • Blank: This system type includes common configuration options.

Custom Applications

  • Blank: This system type includes common configuration options.

Monitoring/Supervisory Control Only

  • Blank: This system type includes common configuration options.

System of Units

Use this option to select the units to use in your new system (Imperial or Metric).

Note: After setting the units and closing the tool, the tool remembers the last units setting. See Unit Preferences in the Setting Preferences section.

OK

Applies the selections and closes the dialog box. The System Selection Wizard appears.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.