See Configuring the MUX Block.
|
Field |
Description |
|---|---|
| Edit | Use to edit the table data. |
| IO Modifications | Enables you to add or remove inputs and outputs that define the modes buttons in the left pane. |
| Name | Use to enter a name for the block. |
| Object Identifier | Indicates object BACnet ID and instance number. |
| Input and Outputs Table |
Displays both an Inputs and an Outputs table for the selected module/block. These tables include the following data:
|
|
Input 1 - Mode(s) |
Defines the modes that are configured for this input. If the mode value equals one of the input mode configurations, the value on the input is passed. See Mode Selection. |
|
Input 2 - Mode(s) 1 |
Defines the modes that are configured for this input. If the mode value equals one of the input mode configurations, the value on the input is passed. See Mode Selection. |
|
Apply |
Applies the changes. |
|
Cancel |
Discards the changes. |
| Close | Closes the screen. |
|
|
Opens the Help system. |
1 The number of Input X - Mode(s) fields is determined by the number selected in the Input field.