Default Element Selection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See Setting the Default Element of a Module.

Table 1. Default Element Selection

Field

Description

List of Elements

Lists the elements you can select as the default element for the module.

OK

Applies the changes and closes the dialog box. The default element appears with a black background and white text.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.