Expose Ports for Connection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Some items in the lists may appear disabled because they are automatically exposed for connection and cannot be changed, or if they are already connected. See Exposing Ports for Connection and Exposing Ports.

Table 1. Port Exposure (For Connection)

Field

Description

Filter Provides text box to search the selection tree based on the node name. The search results include the matching node and its ancestors.

Input Port List

Lists the input ports you can hide or expose for connections and allows you to select ports using check boxes.

Output Port List

Lists the output ports you can hide or expose for connections and allows you to select ports using check boxes.

Select All

Selects all input/output ports in the Input Port List and Output Port List.

Deselect All

Removes the selection of all input/output ports in the Input Port List and Output Port List.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.