New Module Selection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The New Module Selection screen appears in multiple instances, such as when you add a new item within the Control View, or when you open the Launch Wizard. Table 1 and Table 2 provide information on the differences between adding new module selections and input/output selections. See Creating Custom Logic (Adding Modules) and Using the Launch Wizard.

The following table applies to the New Module Selection dialog box for the following options:

  • Launch Wizard
  • Network Inputs
  • Setpoint/Miscellaneous Module Selection

  • State Generation Module Selection

  • Output Control Module Selection

  • Network Outputs
Table 1. New Module Selection for Modules and Network Inputs/Outputs

Field

Description

Filter

Filters the content of the table. Type one or more letters appearing in the data you want to view.

Count Specifies the number of modules to add to the system.
Name
Lists the default name of the module. This name appears in the UI if you do not specify a User Name.
Note: To open the web help for a module, click the appropriate link in this field.

Palette

Specifies the folder or category that the module is part of.

Standard Name

Displays a Johnson Controls standard name for the module.

User Name

Specify a name for the module.
Note: If this field is blank, the value in the Name column is used.
Previous Disabled for Classic View additions.
Next Disabled for Classic View additions.
Finish Applies changes and closes the dialog box.
Cancel Discards changes and closes the dialog box.

Opens the Help system.

The following table applies to the New Module Selection dialog box for the following options:

  • Inputs
  • Miscellaneous Inputs

  • Outputs
  • Miscellaneous Outputs

Table 2. New Module Selection for Inputs and Outputs

Field

Description

Filter

Filters the content of the table. Type one or more letters appearing in the data you want to view.

Count Specifies the number of points to add to the system.

Application

Lists the application types available for the points.

Function

Lists the functions available for the points.

Data Type

Lists the data types available for the points.

Signal

Lists the signals available for the points.

User Name

Specify a name for the module.

Previous Disabled for Classic View additions.
Next Disabled for Classic View additions.
Finish Applies changes and closes the dialog box.

Cancel

Discards changes and closes the dialog box.

Opens the Help system.