See Modifying an Input or Output Signal.
|
Field |
Description |
|---|---|
|
Current Signal |
Current signal type of the point. |
| Signal Options Filter | Use to enter search criteria for sorting applicable Signal Definitions. |
| Signal Definition |
Use to select a different signal for the input or output. |
| Device Support | Indicates whether or not the hardware in your CAF supports the signal type. |
| Ports Available | Indicates whether or not the hardware in your CAF has available ports to support the signal type. |
| Standard Recommended | Indicates whether the signal type is a standard recommendation for the input or output. |
|
Update |
Applies the change and closes the dialog box. |
| Device Assignment 1 |
To an existing device Assigns the input or output point with a Network Sensor that exists in your CAF. To a new device Creates a new device based on the input or output point and then assigns the point with the new device. For example, if your standard input/output point is ZN-T the tool will create a Network Sensor device to bind your point to. |
| Device List | Displays available devices in the CAF you can bind points to. |
|
Cancel |
Closes the dialog box without applying the change. |
|
|
Opens the Help system. |