See Customizing State Selection Tables.
|
Field |
Description |
|---|---|
|
Name |
Use to type a name for the module/column. We recommend leaving this field empty so that dynamic naming may be used. |
|
Column Index |
Indicates the order in which the column appears in the table. |
|
Column Data Type (Port Type) |
Use to select an Enumeration set to use, or indicates to use a Boolean data type. |
|
OK |
Creates the column and closes the dialog box. |
|
Cancel |
Closes the dialog box without applying the change. |
|
|
Opens the Help system. |