FSM Explorer - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Finite State Machine (FSM) Explorer enables you to view the current state and all potential states of an application. The Current State list displays the current state or pseudo-state, while the Possible Next States columns display the possible next states for the current state.

The FSM Explorer provides additional functionality during Simulation and Commissioning. For further information seeFSM Explorer.

For information about a specific module, see State Generation Modules.

For information on the various ways to view the FSM Explorer, see Viewing the FSM Explorer.