Editing a Broadcast Management (BBMD) Object - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

To edit a Broadcast Management object, complete the following steps:

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. Under the Device Information folder, click BBMD. Information about the object appears in the right section of the screen.
  4. Click Edit. The fields that you can edit appear in white.
  5. Click Modify to edit BM Addresses.
  6. In the BM Addresses screen, use the arrow symbols to change the BM address sequence. To add or remove BM addresses, click the Add or Remove buttons respectively. Click the Details button to view individual BM Address details.
  7. Click Save to save your changes.