Adding a Broadcast Management (BBMD) Object - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

If you open a CAF file that does not have a Broadcast Management object defined, you can add an object using one of the following methods:
  • Click on the Device Information folder and press Insert.
  • Right-click the Device Information folder and select Add BBMD Configuration.
  • Click Select in the Field Device section in Define Hardware. If the selected field device supports BBMD functionality, it appears in the Advanced tab.
  • In the Transfer Summary screen, select an option in the BBMD Enabled list and then select Modify open application with New Information column. The Broadcast Management object appears when the transfer process is complete.